Technical FAQs

Ask a Question

The CCM red light blinks intermittently. Do I have a communications problem?

Not if you are performing mixed mode communications - devices speaking Sy/Max and Modbus protocols on a single daisy chain. In this case the red light will blink intermittently. This is normal operation.
Refer to the CCM Instruction Bulletin 48049-151-xx for various L.E.D. interpretations.



CTA-ID : 9741
Was this helpful?
What can we do to improve the information ?