Technical FAQs

Ask a Question

What is the difference between the Trip Unit Alarm Log and the Breaker Event Log?

The Trip Unit Alarm Log records all alarms occurring in the trip unit. These alarms are auto-uploaded into SMS at the onboard alarm check interval setup with the SMS Configuration utility.

The Breaker Event Log records breaker closed/opened, springs charged, etc. for the breaker itself.

CTA-ID : 9740
Was this helpful?
What can we do to improve the information ?