Technical FAQs

Ask a Question

*****DUPLICATE***** What is the difference between TRIP HISTORY and ALARM HISTORY *****DUPLICATE: SEE FA97979*****

Trip History is the date, time, and cause of the last 10 breaker trips.
Alarm history is the date, time and cause of an advanced protection feature that did NOT cause the breaker to trip.
Example: When an Undervoltage alarm was set up to close an auxiliary contact this would appear in the alarm history but not the trip history.



CTA-ID : 9736
Was this helpful?
What can we do to improve the information ?