Technical FAQs

Ask a Question

Why can you set 2 power flow direction settings on the trip unit HMI?

The trip unit has 2 separate modules: one for metering and the other for protection. They act as 2 separate devices. You must set the direction in both of them. The direction should ALWAYS be set as the same and if it is not errors and confusion will result.

CTA-ID : 9735
Was this helpful?
What can we do to improve the information ?