Technical FAQs

Ask a Question

What are the repair parts for the H463 series F5? (may be shown as F05)

Repair parts

Product Line:
Heavy Duty Safety Switch


The replacement parts for the H463, series F5 (F05) are as follows. No other parts are available.

Interior kit - HSIF4610F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Load base kit - HLB210F (TWO required, includes load base & mounting hardware).
Arc Suppressor kit - HAS0610F - (TWO required, includes arc suppressor & mounting hardware)
Lug kit - AL10F - (TWO required, kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)

CTA-ID : 9992
Was this helpful?
What can we do to improve the information ?