Technical FAQs

Ask a Question

What are the repair parts for the DT322RB, series F5? (may be shown as F05)

The repair parts for the DT322RB, series F5 (F05) are as follows. No other parts are available.
-Line Base - 40566-039-50 (one each upper and lower. Order arc suppressor and wire assembly separately).
-Line Base mounting screws - 40205-151-01 (requires 3 per line base).
-Load Base - 40566-047-50 (one each upper and lower. Order lugs and wire assembly separately).
-Load Base mounting screws - 40205-151-01 (requires 2 per load base).
-Arc Suppressor Assembly - 40566-355-50 (requires 1 per line base).
-Arc Suppressor mounting screw - 40205-145-01 (requires 1 per arc suppressor).
-Wire Assembly - 40566-097-50 (requires 1 per phase. Includes cable factory connected mechanical lug at one end and at other end a crimped connector. Use mounting screws of line and load lugs.)
-Line and Load Lug Assembly - 40251-016-52 (per lug - line, load)
-Line, Load Lug mounting screw - 40205-142-02
-Ground Lug - 40251-016-52 (per lug).
-Ground Lug mounting screw - 40205-135-03
-Switch Mechanism - 40566-469-50 (each for upper and lower).
-Linkage Assembly - 40566-149-50 (links together upper and lower switch mechanisms). Also replace linkage assembly rubber gaskets.
-Linkage Assembly Rubber Gaskets - 40503-228-01 (3 total required)
-Linkage Assembly mounting screws - 22999-405-62 (requires 7).
-Handle - 40566-887-50 (In addition, handle gasket required. Lockplate gasket may also need replacing)
-Handle gasket - 40566-086-01
-Lockplate - 40566-733-01 (In addition, lockplate gasket required.)
-Lockplate gasket - 40566-086-01 (requires 1)
-Lockplate mounting screws - 22999-405-62 (requires 2).



CTA-ID : 9905
Was this helpful?
What can we do to improve the information ?