Technical FAQs

Ask a Question

What are the repair parts for the H322NRB, series F5? (may be shown as F05).

Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Cause:
Maintenance

Resolution:
The replacement parts for the H322NRB, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly -40566-420-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 4056002550K (requires one per switch)
Arc Suppressor Assembly - HAS0610F
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Neutral Assembly - SN03
Neutral Bonding Screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)
Line & Load base mounting screws - 40205-160-01 (3 for line & 2 for load)
Arc suppressor mtg screw - 40205-145-01 (1 required)
Lockplate mtg. screw - 22999-405-62 (2 required)


CTA-ID : 9971
Was this helpful?
What can we do to improve the information ?