Technical FAQs

Ask a Question

Are replacement contacts available for 8910DPA92?

Issue:
Are replacement contacts available for 8910DPA92?

Product Line:
Definite Purpose Contactors

Environment:
Products sold and used in the United States

Cause:
Replacement Contacts Needed

Resolution:
In single pole kits only, order (2) 9998 DRC9 kits.


Note: Digest 173 indicates the replacement contact kit for these contactors is 9998 DRC12, this is in era as there is no DPA80. The DPA80 should be DPA90 and the last item marked DPA90 should be DPA120 which uses the 9998 DRC12 contact kit.



CTA-ID : 9893
Was this helpful?
What can we do to improve the information ?