Technical FAQs

Ask a Question

What are the part numbers for the two wiring compartment covers for the 5A and 6A enclosures of the encapsulated dry type transformer? (Key words: replacement cover buck boost low voltage)

The wiring compartment of the encapsulated transformers requires two pieces:
1) the small cover with the knock outs is part number 39002-288-04
2) the large cover without knock outs is part number 39002-287-04
These can be ordered through any Square D Field Office.

CTA-ID : 9674
Was this helpful?
What can we do to improve the information ?