Technical FAQs

Ask a Question

What are the repair parts for a H322DS Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40512-492-50 (arc suppressor NOT included)
Load base assembly - 40512-501-50
Arc suppressor assembly - 40512-421-50
Lug assembly - 40256-034-50
Line and load base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)

CTA-ID : 9253
Was this helpful?
What can we do to improve the information ?