Technical FAQs

Ask a Question

What are the repair parts for a H222DS Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40512-495-50 (arc suppressor NOT included)
Load base assembly - 40512-503-50
Arc suppressor assembly - 40512-445-50
Lug assembly - 40256-034-50
Line and load base mounting screws - 40205-065-01
Handle knob kit - 4028344050K ( Series E Switches only)


CTA-ID : 9252
Was this helpful?
What can we do to improve the information ?