Technical FAQs

Ask a Question

Can a sub-feed breaker be added to a NQOD panel that is already out in the field?

There isn`t any way to add this in the field if a subfeed breaker assembly doesn`t already exist. If the panel is a 400A or 600A and there is an already existing sub-feed breaker, a second sub-feed breaker can be added in the field.


CTA-ID : 9658
Was this helpful?
What can we do to improve the information ?