Technical FAQs

Ask a Question

What does it mean when an ATV66 display shows the image of a keypad and a drive with a line between the two and an X across the line?

This indicates a link fault or keypad link fault (not to be confused with a serial communication link fault). This means communication between the keypad and the control board has been interupted. It may be the keypad is mis-seated, there is a loose keypad cable (if applicable), the control board of keypad has malfunctioned, or there is a power board issue. Each of these should be checked in turn to isolate.

dup of 9400


CTA-ID : 9399
Was this helpful?
What can we do to improve the information ?