Technical FAQs

Ask a Question

What are the repair parts for a HU361AEI Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40566-672-50 (arc suppressor NOT included)
Arc suppressor assembly - 40566-694-51
Lug assembly - CL0306F (includes 6 lugs)
Line base mounting screws - 21427-171-61
Arc suppressor mounting screws - 40205-071-01
Handle knob kit - 4028344050K ( Series E Switches only)
Electrical interlock kit - EK3001 or EK3002

CTA-ID : 9244
Was this helpful?
What can we do to improve the information ?