Technical FAQs

Ask a Question

PDC4LA250: What are the torque and wire requirements?

Mounting screw torque: 180 lb-in.
Conductors: 3 maximum
Size: 250 kcmil Cu at 190 lb-in.
#1-#4/0 AWG Cu at 130 lb-in.
#2 AWG Cu at 60 lb-in.
#6-#2 AWG Cu at 40 lb-in.
#14-#8 AWG Cu at 35 lb-in.


CTA-ID : 9639
Was this helpful?
What can we do to improve the information ?