Technical FAQs

Ask a Question

PDC6KA4: What is the torque and wire specifications?

Mounting screw torque: 80 lb-in
Conductor: 6 maximum
Size: #6-#4 AWG Cu at 35 lb-in
#8 AWG Cu at 25 lb-in
#14-#10 AWG Cu at 20 lb-in

KEY WORDS: POWER DISTRIBUTION CONNECTOR LUG


CTA-ID : 9636
Was this helpful?
What can we do to improve the information ?