Technical FAQs

Ask a Question

PDC3KA20: What are the torque and wire specifications?

Mounting screw torque: 80 lb-in
Conductor: 3 maximum
Size: #4-#2/0 AWG at 50 lb-in
#10-#6 AWG at 45 lb-in
#12 AWG at 35 lb-in
#4-#1 AWG at 40 lb-in
#14-#6 AWG at 35 lb-in

KEY WORDS: POWER DISTRIBUTION CONNECTOR


CTA-ID : 9635
Was this helpful?
What can we do to improve the information ?