Technical FAQs

Ask a Question

PDC6FA6: What are the torque specs and wire size requirements?

Mounting screw torque: 40 lb-in
Conductors: 6 maximum, #8-#6 AWG Cu at 25 lb-in, #14-#10 at 20 lb-in.




CTA-ID : 9634
Was this helpful?
What can we do to improve the information ?