Technical FAQs

Ask a Question

PDC3FA2: What are the torque specs and wire size requirements?

Mounting screw torque: 40 lb-in
Conductor: 3 maximum, #6-#2AWG Cu, at 40 lb-in, #14-#8 AWG Cu at 35 lb-in.


KEY WORDS: Lugs


CTA-ID : 9632
Was this helpful?
What can we do to improve the information ?