Technical FAQs

Ask a Question

Why does an ATV66 Size 6 or 7 drive display overtemperature when then ambient temperature is less than 32 degrees F?

The overtemperature circuit is used to indicate both a high and a low temperature condition. 32F (O degree C) is the minimum operating temperature of the drive; 104F (40 degree C) is the maximum.


CTA-ID : 9396
Was this helpful?
What can we do to improve the information ?