Technical FAQs

Ask a Question

What are the repair parts for a H221AWK Series E1 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40512-609-50 (arc suppressor NOT included)
Arc suppressor assembly - 40512-542-01
Lug assembly - CL0306F (includes 6 lugs)
Line base mounting screws - 21427-171-61
Arc suppressor mounting screws - 40205-082-01
Handle knob kit - 4028344050K ( Series E Switches only)

CTA-ID : 9235
Was this helpful?
What can we do to improve the information ?