Technical FAQs

Ask a Question

Will the Altivar ATV58 Econo-Flex work with Lonworks protocol?<br />

The unit will work with Lonworks protocol if obtain the Lonworks to Modbus option part number VW3A58312PU. The module is then connected point to point through the supplied 29.5 in cable to either the ATV58 integrated keypad MODBUS port or to the 9-pin connector on the Modbuss option card ( part number VW3A58303 ) which comes as part of package when order Lonworks module for Econo-flex.


CTA-ID : 9623
Was this helpful?
What can we do to improve the information ?