Technical FAQs

Ask a Question

What are the repair parts for the H324DS, series F5? (may be shown as F05)

The list of repair parts is needed for Safety Switch catalog number H324DS, series F5.

Product Line:
Heavy Duty Safety Switch

Applicable only to H324DS, Series F5

The repair parts numbers for the H324DS, series F5, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

The replacement parts for the H324DS, series F5 (F05) are as follows. No other parts (enclosure, labels) are available.
Complete Line Base - 4056703350 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020514202 (requires 6 per line base)
Load Base Assembly - 4056678250 (requires one per phase - includes phynolic base, lugs and fuse clips)
Load Base mounting screws - 4020514202 (requires 2 per load base)
Arc Suppressor Assembly - 4053922001(requires one per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires mechanism coupling assembly 40566-998-50 and interlock connector assembly 40567-188-50)
Switch Mechanism mounting screws- 2194918121 (requires 2)
Handle Assembly - 4056736850
Lockplate - 4056738901
Lockplate mounting screws - 2194918121 (requires 2)
Was this helpful?
What can we do to improve the information ?