Technical FAQs

Ask a Question

What is the UL and CSA File # for a 9070 Type T Industrial Control Transformer?

Issue:
What is  the  UL  and CSA File # for a 9070 Type T Industrial Control Transformer?

Product Line:
LV Transformers

Environment:
Applies to Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Industrial Control Transformers have associated UL File numbers

Resolution:
The UL file is # E61239 for all 9070 Type T and TF 25-5000 and EO17-11 and the CSA # is LR37055, guide 184-N-90 for 9070T 25 - 1000VA and all 9070EO types.


CTA-ID : 9608
Was this helpful?
What can we do to improve the information ?