Technical FAQs

Ask a Question

What is the IP fingersafe ratings for 29321 and 29323 terminal covers? These terminal covers go on NS100/160/250.

29321 and 29323 terminal covers are both rated at IP40. The 4 means protection against solid objects greater than 1.0mm and the Zero means no protection against liquid.


CTA-ID : 9606
Was this helpful?
What can we do to improve the information ?