Technical FAQs

Ask a Question

What is the average current draw of a shunt trip for an MA or MH 800 amp 3 phase breaker with a 1021 120 volt shunt trip?<br />

The VA at 120 vac is 24 which draws 0.2 amps.

CTA-ID : 2020124
Was this helpful?
What can we do to improve the information ?