Technical FAQs

Ask a Question

What are the repair parts for the H224N, series F5? (may be shown as F05)

Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to H224N, Series F5

Resolution:
The replacement parts for the H224N, series F5 (F05) are as follows. Only these parts can be replaced. No other parts are available.
Complete Line Base - 4056702950 (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020546401 (requires 6 per line base)
Load Base Assembly - 4056677450 (requires one per phase - includes phynolic base, lugs and fuse clips)
Load Base mounting screws - 4020546401 (requires 2 per load base)
Arc Suppressor Assembly - 4053922001(requires one per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650
Switch Mechanism mounting screws- 2299940562 (requires 2)
Handle Assembly - 4056663550
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (requires 2)
Neutral Assembly - SN20A
Neutral Bonding Screw - 4028356651
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)


 
Was this helpful?
What can we do to improve the information ?