Technical FAQs

Ask a Question

What is the flamability rating for MG26970 padlock attachment? (high temperature rating)

The materiel used is : PA (polyamide)
- 6 - 30 % - FV (glass fibre)
HB class UL
glow wire test : 650 ?



CTA-ID : 9580
Was this helpful?
What can we do to improve the information ?