Technical FAQs

Ask a Question

Define DRAWOUT CIRCUIT BREAKER.

DRAWOUT CIRCUIT BREAKER: a circuit breaker and a supporting
structure designed so the assembly can be moved to either the main circuit
connected or disconnected position without removing connections or
mounting supports.


CTA-ID : 9189
Was this helpful?
What can we do to improve the information ?