Technical FAQs

Ask a Question

Define a circuit breaker.

CIRCUIT BREAKER: a device designed to open and close a circuit
manually and to open the circuit automatically when an overcurrent occurs
without damage to itself when properly applied within its rating. See also
molded case circuit breaker.


CTA-ID : 9185
Was this helpful?
What can we do to improve the information ?