Technical FAQs

Ask a Question

Define AMMETER/TRIP INDICATOR (local current meter/trip indicator).

AMMETER/TRIP INDICATOR (local current meter/trip indicator): a
module that mounts directly to the circuit breaker trip unit. The ammeter
(current meter) reports rms phase and ground-fault current values as
measured by the trip unit. Current values are displayed one phase at a time.
The trip indicator displays whether the circuit breaker tripped as a result of
an overload, short-circuit, or ground-fault condition.


CTA-ID : 9184
Was this helpful?
What can we do to improve the information ?