Technical FAQs

Ask a Question

What is the minimum current required for operation of the QOU aux. switch at 100Vac to 200Vac?

At 100-200Vac, there is good electrical pressure for the switch to work down to 10-20 milliamp level. However, it is a non-sealed switch, and is sensitive to environmental factors (dust, humidity, corrosive atmosphere). Under adverse conditions, the minimum current level would increase. In a clean, dry, temperature-controlled environment, it should be OK at 10-20 mA.

CTA-ID : 9568
Was this helpful?
What can we do to improve the information ?