Technical FAQs

Ask a Question

What does the term ``NEMA Type 5`` refer to?

In Non-Hazardous Locations, the specific enclosure Types refer to the environmental conditions they are designed to protect against. NEMA Type 5 enclosures are constructed for indoor use to provide a degree of protection to personnel against incidental contact with the enclosed equipment; to provide a degree of protection against falling dirt; against settling airborne dust, lint, fibers and flyings; and to provide a degree of protection against dripping and light splashing of liquids. For more detailed and complete information, NEMA Standards Publication 250-1997, ``Enclosures for Electrical Equipment (1000 Volts Maximum)`` should be consulted.


CTA-ID : 9368
Was this helpful?
What can we do to improve the information ?