Technical FAQs

Ask a Question

What are the available rating plugs and settings for the P-frame, R-frame and NS630b - NS3200 Electronic Trip Circuit Breakers?

Interchangeable rating plugs are available to limit the long-time threshold setting range for greater versatility.
For P-frame and R-frame Circuit Breakers
Type A (standard) 0.4 0.45 0.5 0.6 0.625 0.7 0.8 0.9 1
Type B 0.4 0.44 0.5 0.58 0.625 0.75 0.88 0.95 1
Type C 0.417 0.50 0.533 0.583 0.667 0.75 0.933 0.95 1
Type D 0.4 0.48 0.64 0.7 0.8 0.9 0.93 0.95 1
Type E 0.6 0.7 0.75 0.8 0.85 0.9 0.93 0.95 1
Type F 0.84 0.86 0.88 0.9 0.92 0.94 0.96 0.98 1
Type G 0.66 0.68 0.7 0.72 0.74 0.76 0.78 0.8 0.82
Type H 0.48 0.5 0.52 0.54 0.56 0.58 0.6 0.62 0.64

For NS630buNS3200 Circuit Breakers
Type R (standard) 0.4 0.5 0.6 0.7 0.8 0.9 0.95 0.98 1
Type S 0.4 0.45 0.5 0.55 0.6 0.65 0.7 0.75 0.8
Type T 0.8 0.82 0.85 0.88 0.9 0.92 0.95 0.98 1
Type P (off plug) No long-time protection.



CTA-ID : 8857
Was this helpful?
What can we do to improve the information ?