Technical FAQs

Ask a Question

Is MODBUS communications available on circuit breakers with Micrologic Ammeter trip units 3.0A, 5.0A, 6.0A?

Iquiry:
Is MODBUS communication available on Powerpact and Masterpact circuit breakers with Micrologic Ammeter trip units 3.0A, 5.0A, 6.0A?

Product Line:
Powerpact P, R and Masterpact NT and NW circuit breakers

Environment:
Electrical Distribution

Cause:
Selection and upgrade

Resolution:
Yes. To enable MODBUS communication on breakers with the Ammeter trip units, install the BCM (breaker communication module).  Choose it in the product selector or for field installation, order per listing in the Digest or Masterpact Pricing Guide.  Separate 24 Vdc power supplies for the BCM and trip unit are also required.
Was this helpful?
What can we do to improve the information ?