Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the Cradle position switches (CE CD CT) for the Masterpact NT breaker?<br /><br />

Standard: 10 mA/24V minimum load. Max rating:
240 Vac 8 A
380 Vac 8 A
480 Vac 8 A
600/690 Vac 6 A
24/48 Vdc 2.5 A
125 Vdc 0.8 A
250 Vdc 0.3 A


CTA-ID : 8846
Was this helpful?
What can we do to improve the information ?