Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the Connected/Closed Switch (EF) for the Masterpact NW breaker?<br /><br />

Standard: 10 mA/24 V minimum load.
Maximum rating:
240/380 Vac 6 A
480 Vac 6 A
600/690 Vac 6 A
24/48 Vdc 2.5 A
125 Vdc 0.8 A
250 Vdc 0.3 A


CTA-ID : 8842
Was this helpful?
What can we do to improve the information ?