Technical FAQs

Ask a Question

Is the QO48M30DFGPW1 Generator Panel suitable for use as a manual transfer device?

Issue:
Generator Panel Usage

Product Line:
QO Load Centers

Environment:
NEMA 1

Cause:
Used as a Manual Transfer

Resolution:
Yes, it is labeled as ``MANUAL TRANSFER EQUIPMENT SUITABLE FOR USE IN ACCORDANCE WITH ARTICLE 702 OF THE NATIONAL ELECTRICAL CODE, ANSI/NFPA 70``.
NOTE: This QO48M30DFGPW1 Generator Panel an Obsolete and no longer in production.



CTA-ID : 9561
Was this helpful?
What can we do to improve the information ?