Technical FAQs

Ask a Question

Does the Altstart ATS46 have phase loss detection?

Yes. The unit will detect loss of current to motor on one or more phases and loss of input voltage. It will stop running and display PhF fault.


CTA-ID : 9554
Was this helpful?
What can we do to improve the information ?