Technical FAQs

Ask a Question

What is the isolation function with respect to circuit breakers?

The operating handle is representative of the position of the main contacts. The OFF position can be reached only when the main contacts are fully opened.


CTA-ID : 9162
Was this helpful?
What can we do to improve the information ?