Technical FAQs

Ask a Question

What is the function of the shunt trip for the Powerpact P-frame, R-frame, and NS630b - NS3200 electronic trip circuit breakers?

The shunt trip provides a means of tripping the circuit breaker electrically from a remote location using an external voltage source. The shunt trip may be supplied continuously or intermittently. Communication versions of the shunt trip are available for direct connection via the circuit breaker communication module (BCM).


CTA-ID : 8831
Was this helpful?
What can we do to improve the information ?