Technical FAQs

Ask a Question

Is the MAHEX handle extension required for use with the HPAXLM handle padlock attachment?

Yes. However, the handle extension can be used by itself without the handle padlock attachment.


CTA-ID : 8806
Was this helpful?
What can we do to improve the information ?