Technical FAQs

Ask a Question

What is the minimum current requirement for the QOU aux. switch at 100Vac or 200Vac?

The switch will work down to 10-20mA at 100-200Vac when new. But longevity depends on environmental factors (dust, humidity, corrosive atmosphere or not).


CTA-ID : 9545
Was this helpful?
What can we do to improve the information ?