Technical FAQs

Ask a Question

What class or type of fuses are used in the L221N Light Duty Safety Switch?

Issue:
Product design features

Product Line:
Light Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:
This switch accepts Class H fuses. The switch is UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 9544
Was this helpful?
What can we do to improve the information ?