Technical FAQs

Ask a Question

How can I get high-amp lugs put on a low-amp HOM breaker?

Use suffix 5219 to get high amp lugs on low-amp QO or HOM breakers.
UL APPROVED FOR QO 10-30 AMP ONLY
UL APPROVED FOR HOM 15-30 AMP ONLY


CTA-ID : 9337
Was this helpful?
What can we do to improve the information ?