Technical FAQs

Ask a Question

How can I get high-amp lugs put on a low-amp QO breaker? Customer wants to use large wire to minimize voltage drop.

Use suffix 5219 to get high amp lugs on low-amp QO or HOM breakers.
UL APPROVED FOR QO 10-30 AMP ONLY
UL APPROVED FOR HOM 15-30 AMP ONLY


CTA-ID : 9332
Was this helpful?
What can we do to improve the information ?