Technical FAQs

Ask a Question

What alarm history information is available with the Micrologic P and H trip units?

The last ten alarms are recorded a history file that can be displayed on the screen. The following information is contained in this file:
Type of alarm
Date and time of the alarm
Values measured at the time of the alarm

CTA-ID : 8773
Was this helpful?
What can we do to improve the information ?