Technical FAQs

Ask a Question

What is the allowable padlock shackle diameter for 28050, 28051, 28052, 28053 directly mounted and door mounted rotary handles which are used on NSE breakers?

0.19 to 0.31 inch (5 to 8mm)


CTA-ID : 9150
Was this helpful?
What can we do to improve the information ?