Technical FAQs

Ask a Question

How does a magnetic-only trip unit work?

Magnetic (instantaneous only) trip units are used for short circuit protection only, usually in motor circuits. They have no long-time characteristic and will not trip below the instantaneous trip current, which is usually an adjustable setting.


CTA-ID : 8726
Was this helpful?
What can we do to improve the information ?