Technical FAQs

Ask a Question

Can 2 QO250GFI be installed in series ?

They could be provided the pigtail in the downstream breaker is not bonded there ...instead it should be brought back to the neutral w/ the upstream breaker

CTA-ID : 9132
Was this helpful?
What can we do to improve the information ?